Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What does an OLF fault mean on the ATS22 soft starters?

OLF means motor overload fault.


Remedies:
1- To reset the fault you can go into the Pro menu find ITH set this to OFF  power cycle then set it to ON.
This will reset the OLF fault, Otherwise you have to wait for it to time out and reset on its own.

2-Check the motor for blockage, phase rotation.. etc.

3- Check the ACC and tHP settings in SET menu, if ACC= 10 seconds or more,  try adjusting  the tHP to class 20 or class 30.