Issue:
CRF2 fault on an ATV61 or ATV71 drive.
Product Line:
Altivar ATV61 and ATV71
Environment:
All
Cause:
Thyristor is not ramping DC bus voltage up, Main control board or soft charge board.
Resolution:
Run the thyristor test in menu 1.10 under (Test Procedures).
Replace the Thyristors and/or soft charge board (based on frame sizes).
Replace the power board.
Replace the main control board.
Released for:Schneider Electric Egypt and North East Africa