Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the maximum distance the motor can be from the ATV61 and ATV71 drive?


Issue:
is there a maximum distance of the cables connected between the drive and motor?

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
Application notes on motor cable distance.

Resolution:
Length of motor cables from ATV61


Length of motor cables from ATV71

Length of motor cables from ATV71
Length of motor cables from ATV71

Schneider Electric Egypt and North East Africa