Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the function of the ACP control plate in ATS system ?
The control plate provides in a single unit: •protection for the BA or UA controller with two highly limiting P25M circuit breakers(infinite breaking capacity) for power drawn from the AC source) •control of circuit-breaker ON and OFF functions via two relay contactors •connection of the circuit breakers to the BA or UA controller via a built-in terminal .