Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the best motor control type in ATV71 for a motor application that runs screw by gearbox ?
It is better to use :
  • "SVC I" or "SVC V" for better torque performance, taking into consideration that the drive auto-tuning must be done while using the drive with SVC I & SVC V.
  • "V/F" control can be used also, If the motor cable length is long or the motor is very old or several motors connected in parallel in the same drive.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center