Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What are the causes of a drive overload which is connected to a motor that runs a screw by gearbox ?
The problem of over loading observed may be due to any of below reasons:
  1. If it is a screw extruder, there may be extrusion material struck in the screw, which can cause over loading, if so the same to be cleaned before re-starting the screw extruder.
  2. There is a possibility of jamming or damage of gears or bearing jamming in gear box, which can also cause over loading.
  3. If it is a new drive under installation and you are facing problem, it may be due to inadequate drive rating selection.

Schneider Electric Egypt and North East Africa