Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
How can we connect a PC running SoMOve software to the ATV71 ?
The software can use a direct USB/RJ45 cable link or communicate via a Bluetooth®
wireless link with the drive equipped with the Modbus-Bluetooth® adaptor
(TCSW AAC13FB).