Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
nSt Appears on ATV58 .. What is this error ? how to fix it ?

1. NST is not as fault or error. It is a status of drive like, ACC, DCC, RUN etc...(NST means, the drive is in free wheel stop mode)
2. Most of the cases, it can happen due to any of loose connection or wiring disconnection in Logic input wiring (LI1 or LI2 etc..)
3. It can also happen due to failure of power board. Please check the +24VDC is available in Drive terminal. If the +24VDC is missing in drive terminal, it can also show "NST"

Suggestions:
1. Check whether the 24VDC is available in drive terminal or not.
2. If 24V is not available at drive terminal, please arrange to replace the power board and control bard.
2. If 24V is available, in 3 wire configuration, locally short(with a small wire) the +24V terminal and LI1 terminal and check the drive is showing RDY.
3. If 24V is available, in 2 wire configuration the drive should show RDY with out any of connection.
4. If the drive is showing RDY, you can give run command (LI1 in 2wire or LI2 in 3 wire configuration) and check the drive is working.

5. If the drive is not working after above checking, Please check the drive operation from HMI whether it is working or not. Even If it not working in HMI, you may arrange to replace the drive power board and control board

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: