Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the CFF fault on the ATS48 soft starter and what causes it?

Issue:
What is the cause of the CFF fault on the ATS48 soft starter?

Product Line:
Altistart 48, ATS48

Environment:
All models, all serial numbers.

Cause:
Invalid configuration on power up.  This could be due to a replaced control board or electrical interference that prevents the control board from reading the configuration.

Resolution:
This fault is due to an Internal configuration error.
Complete a Factory Reset by going to drC menu > FCS parameter> change to YES.  Hold Enter button for 2s to complete this reset.  Reprogram the softstart.
Cycle power to the softstart.  Then provide a new run command.
If the fault persists after these steps, replace the control board or Softstart as applicable.