Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Is there in schneider products : a phase sequence relay ? Does it solve the phase sequence failure automaticaly ?

Yes there is , but it is just for monitoring the phase sequence .
When phase sequence , the output contacts are closed
In the event of a sequencing fault or total loss of one or more phases , the relay opens instantly
But it can't correct the fault automaticaly .