Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
How to take a snapshot using vijeo designer and XBTGT ?
You need to activate the "Copy screen" option in the properties of the target

then you must use the variable _ScreenSnapshot.Control to trigger recording is either printing or 2.

For printing, you must also activate the "printer" option in the properties of the target and set the printer type.

There are also 2 other variables that allow you to see the status and error in the screen print

(_ScreenSnapshot.statut, _ScreenSnapshot.error)

Schneider Electric Egypt and North East Africa