Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
I have TSX Nano with software PL7-07 , is it valid to convert from Pl7-07 to Unity Pro ?
There is no converter from UNITY to PL707. therefore we should re-enter the PLC program.
The only converter that exists with PL707 is a conversion to TwidoSuite .