Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the Difference between VW3A3502 and VW3A3503 multi-pump cards ?

Thanks to check the differences as below:

·         The VW3 A3 502 multi-pump card ensures compatibility of pump applications developed for an Altivar 38 drive with an Altivar 61, without reprogramming.

·         The VW3 A3 503 multi-pump card is not compatible with pump applications developed for an Altivar 38 drive.

·         The VW3 A3 502 multi-pump card ensures a complete pumping installation (up to 5 pumps) can be controlled.

·         The VW3 A3 503 multi-pump card ensures a complete pumping installation (up to 4 pumps) can be controlled with a single drive, providing constant pressure.

For more info, thanks to check the Attached document.

Schneider Electric Egypt and North East Africa

Attachment(s)
ATV 61 - Multi-Pump Cards.pdf [148.94 KB]