Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How is the sleep/wake (low speed timeout) programmed on the ATV212 drives?

Issue:
Sleep/wake operation (low speed timeout)  programmed on the ATV212 drives.

Product Line:
Altivar ATV212

Environment:
All

Cause:
Allows the drive to shut off after running at a preset low speed for a preset period of time.

Resolution:
The sleep/wake threshold is defined as LL + F391.
The time period to trigger sleep mode is F256.
If the drive operates at or below the threshold (LL + F391) for a period of time (F256), the drive will decelerate to a stop and flash LStP.  It will remain stopped until the speed reference again exceeds the threshold (LL + F391).  The drive will then accelerate to the new reference.