Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
In which applications should RCCB adjustment be 10 mA or 30 mA ?
The low settings of 10mA and 30mA are for human protection, though the IEC 60364 standards only ask for 30mA. 30mA are mostly used for socket outlets and places of human access.10mA are for Sauna, Swimming pool equipment, etc.
For light fittings and others 100mA is selected and others 300 or 500mA which is called equipment protection or fire protection.