Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Why I Can’t Reset My XPSMC safety controller output ?

There are some Steps that should be done to make sure of the cause of the problem.

Thanks to check the following steps :

· Auto-test (hardware test):

You can reset the configuration of an XPSMC as follows: Disconnect the XPSMC from power supply, press and hold the Reset button while you reconnect the

XPSMC to the power supply. The configuration will no longer be valid however, it is possible to read the configuration from the controller on the computer and revalidate the configuration.

Stage

Description

1

The LEDs located on the housing light up.

2

After 2 seconds, the LEDs switch off for a short time and then on again, since the
Reset button is pressed.

3

Release the Reset button.

  • PWR LED is on
  • CNF LED is flashing
  • Remaining LEDs are off


If the Problem still Exsists , this may due to any of the following:

LED

Color

Description

E In

red

Internal Error
Lights up if an internal error is detected. The safety outputs are immediately deactivated. If the indication is persistent after power cycle and reset then the XPSMC has been damaged and must be replaced.

E Ex

red

External Error
Lights up when an external error is detected, for example in the wiring. Only the safety outputs of the affected inputs are deactivated. When the detected error has been corrected, and the RESET button has been pressed, the corresponding safety outputs become operational again.