Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
How to install Runtime System to HMISTU Series using the USB port ?
  1. Select the USB port for data transmission.
  2. Turn the target machine on.
  3. Confirm that the download cable is connected to the PC USB port, then in the Runtime Installer, click Send.
  4. Do not turn the target machine off during installation.