Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Is the Blokset enclosure certified for seismic zone?
Blokset has increased resistance to harsh environment, for installation in Seismic zones. As an option Blokset benefits from a reinforced framework to guarantee increased resistance to earthquakes (IEC 68.3.3).
Blokset is totally tested switchboard according to IEC61439-2, All tests are certified by ASEFA and LOVAG.it is also well adapted and certified for the harsh environmental conditions of Gulf countries.

Schneider Electric Egypt and North East Africa