Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Is there any document to solve a problem with READ_VAR EFB in Unity Pro 7.0 when using ETG100 Gateway?
Please check the attached technical note to communicate  through the gateway.
See an example in attached help file for device behind gateway if its not a CPU native port then it can be addressed as below :-
R - rack
m -  module
C- ethernet channel number
Modbus device #14 behind Ethernet gateway whose address is 192.168.100.18 on NOE Ethernet link
ST language.  but for FBD its straight as detailed in document.
ADDM('0.3.0{192.168.100.18}41')
ADDM('Ethernet_1{192.168.100.18}41')

Example : syntax will be
'0.1.0{192.168.100.18}41'   - > example  Rack  = 0, module slot  = 1,  channel  = 0
Or may test with 'Ethernet_1{192.168.100.18}41'

Schneider Electric Egypt and North East Africa

Attachment(s)
read var.pdf [906.58 KB]
read var setting.pdf [68.75 KB]