Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What kind of earth leakage device is suitable for VFD?
ELCB's are not recommended to use in output side of Drive and soft starters, because it may cause nuisance tripping due to PWM output form VFD. However for VFD and soft starter, if the application demands to use of an upstream "residual current device" for protection is required by the installation standards, an A-Si type or Class B type device must be used. If the installation involves several drives or soft starters on the same line, each drive must be earthed separately. If necessary, line chokes needs to be provided as recommended in the catalogue to reduce the leakage current.
ELCB can be used on drive input provided.
1) Residual current device of type B (OR) A-Si type
2) Minimum sensitivity of 300mA.

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center