Issue:
Set up for keypad control with ATV61 and ATV71.
Product Line:
ATV61 and ATV71 drives
Environment:
All
Cause:
Running the drive start stop and speed control from the HMI
Resolution:
If normal operation of the VFD is designed for Start/Stop and Reference control to be through the HMI/keypad, program the VFD as follows, under the Drive menu:
1.6 Command menu
Ref 1 channel = HMI
Profile = Separate
Cmd switching = ch1 active
Cmd channel 1 = HMI
Ref 2 switching = ch1 active
1.7 Application Function
Ref 1B switching = ch1 active
Set up for keypad control with ATV61 and ATV71.
Product Line:
ATV61 and ATV71 drives
Environment:
All
Cause:
Running the drive start stop and speed control from the HMI
Resolution:
If normal operation of the VFD is designed for Start/Stop and Reference control to be through the HMI/keypad, program the VFD as follows, under the Drive menu:
1.6 Command menu
Ref 1 channel = HMI
Profile = Separate
Cmd switching = ch1 active
Cmd channel 1 = HMI
Ref 2 switching = ch1 active
1.7 Application Function
Ref 1B switching = ch1 active
Released for: Schneider Electric Egypt and North East Africa