No, the changing of settings remotely is not password protected.
To modify protection settings remotely in Sepam 1000+ through the Modbus communication link, no passwords are required.
The remote setting feature can be inhibited in each Sepam 1000+ (it's one of the parameters of the General settings)
A controlled access to this function have to be programmed in the SCADA system.
The remote setting feature on Sepam 2000 is based on the same principle.
Released for: Schneider Electric Egypt and North East Africa