Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the right way to connect and chain the MET 148, MSA 141, and DSM 303 accessories on the Sepam 20 or 40?

Goals and Symptoms

What is the right way to connect and chain the MET 148, MSA 141, and DSM 303 accessories on the Sepam 20 or 40?

Causes and Fixes


On the D Port you have to connect and chain in order:

(1) MSA 141

(2) MET 148 ( Attention: Option 2 MET 148 for Sepam 40 only )

(3) DSM 303 (Always at the end of this chain and only if no more than 2 accessories already connected on Sepam)

Note: you can't connect more 3 accessories on this chain so if you already have 1 MSA 141 and 2 MET 148 it is impossible to set also 1 DSM 303. In this case if you want to put this DSM 303, you have to remove the MSA 141 or 1 MET 148.

Key words and phrases: MSA141, MET148, DSM303

AEDL3


Legacy KB System (APS) Data: RESL201098 V1.0, Originally authored by DaMi on 01/22/2010, Last Edited by DaMi on 01/22/2010
Related ranges: Sepam accessories, Sepam series 20, Sepam series 40