{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Which protocols can be used on the SLAN output (Fiber optic output) of ACE969FO-2?


Since the ACE969FO-02 does not have an Ethernet port, you cannot be connected to Ethernet using the ACE969FO-2. The S-LAN output of the ACE969FO-2 is a serial port that supports Modbus RTU or DNP3 or IECI 60870-5-103 protocols (but obviously not Modbus TCP/IP since this is an Ethernet protocol). To communicate Modbus TCP/IP, use the ACE850FO. For more information, there is a chart in the "Communication Accessories" section of the Sepam 20, 40, 80 "Digital Protection Relays" catalogue. A copy of this chart from the 2010 version of this catalogues is reproduced below for convenience:



Keywords: Ethernet communications, serial communications, fiber ethernet, fiber serial, fiber optic, connection port, support, Modbus RTU over Ethernet, DNP over Ethernet, IEC103, Modbus TCP

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.