Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: How to separate the ANSI 50 (Instantaneous phase over current) from the ANSI 51 (delayed phase over current) protection on a SEPAM digital relay offers ANSI 50/51 over current protection.

Issue
Need to program the SEPAM for instantaneous and curved (IDMT) over current protection.

Product
SEPAM 20
SEPAM 40
SEPAM 80

Resolution
The ANSI 50/51 protection option in SEPAM relays combine both ANSI 50 instantaneous phase over current protection and ANSI 51 delayed phase over current protection.
In order to activate ANSI 50 protection, an instantaneous delay of 0 ms must be set for the time delay. Confirmed instantaneous operation times are:

inst. < 50 ms at 2 Is for Is >= 0.3 In (typically 35 ms)
inst. < 70 ms at 2 Is for Is < 0.3 In (typically 50 ms)
Setting Group A


In order to activate ANSI 51 protection, a delay greater than 50 ms must be set for the same parameter setting time delay. This will allow the end-user to use ANSI 51 delayed phase over current protection.

Setting Group A 2

Below is a video to help program the basic needs for over current protection using circuit breaker control featuring the SEPAM™ 20 Series as an example: