XBTL100 A second EQUIPMENT is available but button is NOT active in the Dailog table
Goals and Symptoms
Adding an EQUIPMENT table in the Configure Dialogue table screen. "Use Dialogue Table" is selected. A second EQUIPMENT is available. Is shown and selected in "EQUIPMENT available" list. But "Add table" button is NOT active
Facts and Changes
XBTL1000
Causes and Fixes
When you add an other EQUIPMENT , you can only use the alarm table function.
Now, the alarm table capacity is limited to 64 words. If this capacity is reach by the main EQUIPMENT, there is no more space to create an other one for a secondary EQUIPMENT. Then the "Add Table" button is not active.
Released for: Schneider Electric Egypt and North East Africa
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.