Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Getting a USF fault on an ATS soft start (ATS46, ATS48, ATS430, ATS480, ATS490)

Issue:
A customer is intermittently getting a USF fault on an ATS softstart when trying to start.
Product Line:
ATS46
ATS48
ATS430
ATS480
ATS490

Environment:
All
Cause:
Faulting on USF
Resolution:

USF is a Supply Mains UnderV error.

The softstart will display 'USF' fault when you have a run command but there is low or no line power present on ATS.

On systems that use an input contactor (also known as an Isolation Contactor) this can occur if the contactor does not close within 200 ms of the start signal.
Check the programming of the R1 relay (normally set to Isolation when used in this manner) and verify the operation of the contactor and any interposing relays.

Newer ATS units (ATS480, 490 and 430) have some adjustment to the undervoltage threshold and UV detection delay that can be reviewed to help ride through power dips while in a running state.

“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)


Schneider Electric Egypt and North East Africa