TSXSCY21601: Channel 0 is not working if a PCMCIA is configured and not present on Channel 1
Goals and Symptoms
TSXSCY21601 module with a PCMCIA card (TSXSCP111 or TSXCP114) configured in the application (PL7 or Unity Pro).
If the card is not physically in the slot (channel 1), the built-in link (channel 0) does not work.
The module is on error with ERR led flashing.
Causes and Fixes
This a normal behavior of the TSXSCY21601 module.
The module can not work if one channel has a default.
Released for: Schneider Electric Egypt and North East Africa