Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can I introduce a control character "carriage return" in a String? String = "message"+ CR (carriage return)

Goals and Symptoms

How can I introduce a control character "carriage return" in a String?

String = "message"+ CR (carriage return)

Facts and Changes

Vijéo-Designer V4.2

Causes and Fixes

In Java, the "carriage return" character is "\n". So, to insert a carriage return into a string, use this character in a string concatenation expression.
The file name is: "carriage return.zip".
The script action inside the switch, You will see the syntax for string concatenation and how the carriage return character is used.
carriage return.zip