Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there a battery backup for the M340 controllers?

Issue:
M340 battery backup


Product Line:
M340


Resolution:
No. The program for an M340 controller is stored on a Memory card so no battery backup is required.