Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the Serial Communication protocol of an M340 PLC be changed dynamically?

Yes the Serial Communication can be changed dynamically from Modbus Master, Modbus Slave, or Character mode by using a WRITE_CMD (%MWr.m.c.24.bit) and toggling bits 12, 13, or 14 respectively.
Example:
1) Bit 12 = 1, bits 13 & 14 = 0 Current protocol is changed to Modbus Master
2) Bit 13 = 1, bits 12 & 14 = 0 Current protocol is changed to Modbus Slave
3) Bit 14 = 1, bits 12 & 13 = 0 Current protocol is changed to Character Mode

Schneider Electric Egypt and North East Africa