Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the serial cable to connect an XBTN200, XBTN400 and XBTR400 HMI to a Modicon M340?


The XBTZ9980 cable allow the communication between Modicon M340 PLC series through Modbus RJ45 port and the following HMI PRODUCTS: XBTN200, XBTN400 and XBTR400.


-Specifications:
cable
-Connectors
XBT side J1 : RJ45 Male 8 points
PLC side J2 : RJ45 Male 8 points

-Length
2.5m

-Temperature
Working temperature : -20°C to +70°C
Storage temperature : -40°C to +80°C

-Certification
CE certified and CSA UL508
Fireproofing rating : UL VW-1 for the cable
ROHS compliance

Schneider Electric Egypt and North East Africa