What is the maximum number of client and server connections on an ETY4103/5103
Issue
What is the maximum number of client and server connections on an ETY4103/5103
Product LIne
TSXETY4103 and TSXETY5103
Environment
Windows 7
Resolution
The following applies to exec fimrware version 4.xx and higher of the 'TSXETY4103' and 'TSXETY5103':
- The ETY4103/ETY5103 has a limit ot 64 connections.
- The connections can be a combination of both client and server. (i.e., 16 clients and 48 server, etc.) .
- 16 of the connections are dedicated for the client.
- There is a limit of 64 connections regardless of the type of connections (i.e., HTTP, TCP, etc.).
- When counting client connections, consideration must also be given for other client connections
- There can be up to 64 connections open but, only 16 simultaneous client connections can be running
connection will be reserved for listening.
Released for: Schneider Electric Egypt and North East Africa
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.