In a Quantum RIO Network, using 140CRP93100 module, PV<08 with 140CRA93X00 modules with PV=09 and DOM<1102 is causing an increase of the RIO Communication Error .
Release Notice
This Resolution follows the 204138 one, some modification and add of binary Q201.bin file has been released.
05/01/2012 : add on of the compatiblity rules
Goals and Symptoms
In a Quantum RIO Network, using 140CRP93100 module, PV<08 (non RoHS design) with 140CRA93X00 modules, PV>=09 (RoHS design), is causing an increase of the RIO Communication Error counters (global communication error words: %SW542 to %SW544, and status of the decentralized stations: %SW548 to %SW640).
Facts and Changes
Cause :
Root cause of the issue is a bad synchronization (in reception) of one component mounted on 140CRA93X00 RoHS PRODUCTS when non RoHS 140CRP93100 is sending some initializing frames.
Only 140CRP93100 non RoHS product can send this kind of frames.
Causes and Fixes
| Block *: | Causes and Fixes |
either change the 140CRP93100, PV< 08 (non RoHS design), for a new 140CRP93100, PV>=08 (RoHS design).
or upgrade the FW of the 140CRP93100 PV<08 using the following attached file :Qcrpv201.bin
Caution: Qcrpv201.bin file is:
- only for a workaround, this will not be delivered in a product from =S=. So this will not delivered in Planet .
- doesn't work with S800 series .
Fix:
So far the fix is included in the produced versions of the 140CRA93100 and 140CRA93200 with the following tracability indexes:
PV >= 9
SV >= 2.0
RL >= 01 (printed on the top of the housing)
DOM >= 1102.
CRP/CRA/S800 .... Compatiblity rules is provided below .
As soon as a new module will be implemented in a PLC configuration, please refer to this excel file to see if the compatibilty is supported, in case of problem contact the support with a description of the problem and the list of the PV and SV of the modules .
Single or HSBY configuration is described.
Attachements
Exec v2.01 (qcrp201.bin) 12/09/10 This version provides a workaround regarding the problem of mixed CRA/CRP : CRP non RoHS and CRA RoHS.
(Removed File URL: 204828_12FE/QCRPV201.BIN)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/216bfc64a56bbaafc1257988002c0d1e/fl_block_5/0.646?OpenElement&FieldElemFormat=gif)
Compatiblity rules: (Removed File URL: 204828_12FE/CRP-CRA_compatibilty.xls)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/216bfc64a56bbaafc1257988002c0d1e/fl_block_5/0.1248?OpenElement&FieldElemFormat=gif)
Legacy KB System (APS) Data: RESL204828 V3.0, Originally authored by ErBe on 03/16/2011, Last Edited by ErBe on 01/17/2012
Related ranges: Modicon Quantum
Released for: Schneider Electric Egypt and North East Africa
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.