Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What cable is used to connect a Harmony/Magelis HMI via RJ45 cable to Zelio Smart Relay Modbus module SR3MBU01BD?

Issue
What cable is used to connect a Harmony/Magelis HMI via RJ45 cable to Zelio Smart Relay Modbus module SR3MBU01BD?

Product Line
Zelio SR3 Smart Relays
HMI families with RJ45 ports: HMISTU, HMISCU, HMIGTO, HMIGTU, HMIST6, HMISTO715

Environment
Modbus Communication hardware

Resolution
Part number to connect Zelio Logic SR3 RJ45 (RS485 Modbus) to the RJ45 port of the HMIs from these families: HMISTU, HMISCU, HMIGTO, HMIGTU, HMIST6, HMISTO715 is either:
XBTZ9980 (2,5 m), or
XBTZ9982 (10 m).

These two cables have the same pinouts, but have different lengths.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Product: