Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible using PRINT_CHAR to write a NULL (0x00) out M340 serial port?

Yes, it is possible using PRINT_CHAR function block to write a NULL (0x00) out the port.
You must just define the number of character to send to include the NULL character and place the NULL character in your string.


Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center