Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why am I getting an error message: "PLC return error code FDH-83,80H" when communicating between a Magelis and a Unity Quantum PLC?

Issue:
Getting an error message: "PLC return error code FDH-83,80H" when communicating between a Magelis and a Unity Quantum PLC


Product Line:
Vijeo Designer, Quantum PLC


Resolution:
The error message is due to the Magelis reading the discrete/analog inputs as %I or %IW from the Unity Quantum. You will need to delete the tags and link to the Unity database file. Then re-link the tags back into Vijeo Designer and check the box to "force IO to unlocated variables". Or convert all of the input variables to memory bits and words.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center