In the attachment file, you will find a presentation which shows an easy way to configure the communication between Lexium Controller and OPC.
This example is based on the freeware:
MatrikonOPC Explorer
You can find it here:
http://www.matrikonopc.com/
Remark: Any other OPC software can be used.
Legacy KB System (APS) Data: RESL192210 V1.0, Originally authored by MaPr on 06/26/2008, Last Edited by MaPr on 06/26/2008
Related ranges: Lexium Controller
Released for: Schneider Electric Egypt and North East Africa