Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
The motor does not have enough torque; it can be stopped with ease.

Possible problem and solution:

Be sure to check your motor run current setting (PR RC)-the default is 25%.
At stand still, the holding torque (PR HC) has a default setting of 5%.
If there is not enough torque, increase the percentage for more torque.


Legacy KB System (APS) Data: RESL200106 V1.0, Originally authored by MaPr on 09/25/2009, Last Edited by MaPr on 09/25/2009
Related ranges: Lexium ILT, ILP