Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can we drain the gear oil in an ILE1B661TC1A8? What is the reference of the gear oil? --------------------------------------------------------------...

Goals and Symptoms

Can we drain the gear oil in an ILE1B661TC1A8?
What is the reference of the gear oil?
-------------------------------------------------------------------
Peux t'on vidanger l'huile du réducteur d'un ILE1B661TC1A8 ?
Quelle est la référence de l'huile du réducteur ?

Causes and Fixes

Klüberplex BEM 34 - 132 special grease ( see attachment )

Attachments

(Removed File URL: 202985_FB46/Kl_C3_BCberplex_BEM34-132.pdf)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/78593e61bc029fd0c12577730052a84a/fl_block_5/0.602?OpenElement&FieldElemFormat=gif)


Legacy KB System (APS) Data: RESL202985 V1.0, Originally authored by VoKo on 08/02/2010, Last Edited by VoKo on 08/02/2010
Related ranges: Lexium ILA, ILE, ILS

Schneider Electric Egypt and North East Africa

Attachment(s)
Kl_C3_BCberplex_BEM34-132.pdf [165.7 KB]