{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How can a Vijeo Look V2.6 authorization be transferred to another computer?

Legacy FAQ.  This product is obsolete and is no longer supported or be authorized.
1. Install Vijeo look on the destination PC.
2. Get the Installation code from the destination PC (Do not turn off the PC because it will generate a new Installation Code)
3. You will need to enter the Serial Number and Reference Number before you can get the installation code available in the orange envelop included
with the CD package.
4. Go back to the source PC to the License Manager. Click on "Transfer Protection" and enter the installation Code generated by the destination PC.
5. Click on "Get Authorization Code" to generate the authorization code for the destination PC.
6. Copy and paste the Authorization code into the destination PC to avoid any typing error.
7. Vijeo Look is now authorized on the destination PC.


Schneider Electric Egypt and North East Africa

Explore more
Range:
E30 series Faceplate
Explore more
Range:
E30 series Faceplate
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.