Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
There is somthing confusing about the current derating with the altitude > 1000m. The data in catalogue is 2.2% per additional 100m while in manual ...

Goals and Symptoms

There is somthing confusing about the current derating with the altitude > 1000m. The data in catalogue is 2.2% per additional 100m while in manual is 0.5%.
Which one is right?

Facts and Changes

ATS48
Altitude

Causes and Fixes

These both values are bad. The real derating is 2% per additional 100 meter.


Legacy KB System (APS) Data: RESL156259 V3.0, Originally authored by on , Last Edited by on
Related ranges: Altistart 48

Schneider Electric Egypt and North East Africa