Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What AC powered inductive device can be used with a Quantum relay module?

Issue

How can I determine if an AC powered inductive device can be used with a Quantum relay module?

Product Line
Quantum

Resolution


Published VA ratings can be used to determine if a product may be used.

Maximum contact current is 2A for the 140DRA84000 and 5A for the 140DRC83000.

The maximum 120VAC load VA rating for the DRA module is 120 x 2 = 240VA.
The maximum 220VAC load VA rating for the DRA module is 220 x 2 = 440VA.
The maximum 120VAC load VA rating for the DRC module is 120 x 5 = 600VA.
The maximum 220VAC load VA rating for the DRC module is 220 x 5 = 1100VA.


Legacy KB System (APS) Data: RESL164212 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modicon Quantum