Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the difference between the Quantum 140CRP93100 and 140CRP93200 Remote I/O modules?

Issue
What is the difference between the Quantum 140CRP93100 and 140CRP93200 Remote I/O modules?

Product line
Modicon Quantum

Environment
140CRP93100

Resolution
The main physical difference is the external connection. The 140CRP93100 has only one channel. The 140CRP93200 has two channels. The following chart lists the specification differences:

texttext
140CRP93100
text
140CRP93200
text
Bus Current Required
text
600 mA
text
750 mA
text
Power Dissipation
text
3 W
text
3.8 W