Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the differences between the ProWORX 32 Full and Lite packages

The ProWORX 32 Full and Lite packages have the same functionality. There are no differences/limitations between the two packages other than the PLC s they support.
372SPU78001PDEV.....ProWORX 32 Full Offline/Online Client Package (supports all of the Momentum, Quantum, 984 Series Slot Mount, Compact, Modicon Micro 110CPU, Modicon Micro984, 984A,B,X Chassis Mount, Atrium and VME controllers).

372SPU71001PLDV.....ProWORX 32 Lite Offline/Online Client Package (only supports all of the Momentum, Compact and Modicon Micro 110CPU controllers).