Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Error "proworxaddrused.frm" when trying to open a Project after installing 'Proworx 32'

Issue
The error "proworxaddrused.frm" gets returned when trying to open a project

Product Line
All versions of Proworx 32

Environment
Windows 7, Windows 10

Resolution
This error will get returned if you updated to a patch immediately after installing 'ProWORX 32' without
rebooting the PC.

To resolve the problem,

  • Insert the installation CD and start the install process.
  • Select the repair option to perform a repair.
  • Reboot the PC.
  • Apply the patch update.

Schneider Electric Egypt and North East Africa