Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
STBXTS5510 Connector Pinouts

Issue

The purpose of this resolution is to document pinouts for the STBXTS5510 HE10 connector used with the STBDDI3725 16 Channel Input module.

Product Line
Advantys, STB

Resolution

connector pin details

Causes and Fixes

See Facts and Changes for the pinout information.


Legacy KB System (APS) Data: RESL190497 V1.0, Originally authored by WeDa on 12/29/2007, Last Edited by WeDa on 12/29/2007
Related ranges: Advantys STB