Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Importing a Modsoft program returns 'Convert' error

Issue
Importing a Modsoft program returns 'Convert' error.

Product Line
ProWORX 32 version 2.1

Environment
Windows 10

Resolution
Importing a Modsoft program returns 'Convert' error:
sd

which is followed by:
fghm

The error will get returned if the Modsoft program contains a custom loadable. To resolve the
problem,

  • Delete the custom loadable from the program using Modsoft
  • Save the changes.
  • Import it the Modsoft program using ProWORX 32'.

During the import, you may get the following warning message because the converter does not
recognize the custom loadable block that is in the logic. You should compare the logic from the
Modsoft program against the 'ProWORX 32' project to ensure that everything is fine with the
exception of the deleted custom loadable nodes or blocks.
fg