Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can I convert a Vijeo Designer toolchest object into a bmp of jpg file without loosing picture quality?


1) Drag the toolchest image of choice onto the panel.
2) Select the image
3) Right Click and select copy.
4) Open Microsoft Word
5) Paste the image in MicroSoft Word
6) In Microsoft word select the image
7) Right click and select copy
8) Open MS Paint and paste the image.
9) Save the image as BMP or JPG.