Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Illumination power and service life for XVBL0M5 .

Goals and Symptoms

Illumination power and service life for XVBL0M5 .

Facts and Changes

XVBL0M5

Causes and Fixes

The life time is 100 000 hours without maintenance (11 years continuous operation).
The values given are an average for all colors.
230 cd/m² without light diffuser.
With light diffuser 140 cd/m²


Legacy KB System (APS) Data: RESL197903 V1.0, Originally authored by LaBe on 02/27/2009, Last Edited by LaBe on 02/27/2009
Related ranges: Harmony XVB